Maker.io main logo

Build a Sense HAT Raspberry Pi Digital Clock

235

2022-12-14 | By Maker.io Staff

License: See Original Project

Digital clocks or watches use traditional optoelectronic display technologies like a ‎liquid crystal display (LCD) or a seven-segment light-emitting diode (LED) to ‎provide visual numbers for the time. The Sense HAT-based Raspberry Pi (RPi) ‎Digital Clock uses a matrix of programmable-addressable discrete LEDs that can ‎display various characters, scrolling text, and numbers. With an 8x8 matrix, the ‎Sense HAT provides 64 pixels for displaying visual information. ‎

hat_1‎ ‎

The RPi Sense HAT.‎

With an RPi Sense HAT digital clock device, the user will enter a basic python script ‎command to operate the clock. The current time will be displayed on the Sense ‎HAT LED matrix by tapping the up-arrow key, followed by the enter key. The ‎python script allows a simple Linux command to run the digital clock code on ‎either a Raspberry Pi 3 or 4 single-board computer (SBC) with an attached ‎keyboard. Another option is to secure-shell (SSH) or virtual network connection ‎‎(VNC) to remotely run the application headlessly, without an attached LCD ‎monitor. ‎

In this project, you will assemble and test an electronic timepiece of your very ‎own! ‎

Assembly of the Sense HAT RPi Digital Clock

The assembly process of the digital clock follows. You will take the Sense HAT and ‎place it on top of the RPi. The Sense HAT comes with a 40-pin dual-inline female ‎header connector.‎

place_2

The Sense HAT placement to the RPi.‎

Before assembling the two boards, place a sheet of red transparent plastic over ‎the Sense HAT. This will make it easier to see the info displayed on the LED matrix ‎without it being washed out by ambient light.‎

red_3

Red transparent plastic sheet over the Sense HAT.‎

Then place the Sense HAT onto the RPi. Ensure the Sense HAT is oriented on the Pi ‎as shown below.‎

final_4

The Sense HAT to the RPi final assembly.‎

Now let’s run a simple test to ensure the two boards are operating correctly. Turn ‎on your RPi, and a colorful visual pattern should be displayed on the Sense HAT. ‎This visual display is analogous to power up the RPi attached to an LCD monitor.‎

color_5

The Sense HAT power-up color pattern

Adding the Sense HAT Digital Clock Code

Before the Python code can be added to the RPi, a few preliminary steps ‎regarding the operating system (OS) for the SBC are required. The first step is to ‎ensure the RPi has the latest OS. Open a terminal and type the following Linux ‎commands to upgrade the OS to the latest version of Raspberry Pi OS. ‎

Copy Code
sudo apt update
sudo apt upgrade

The Sense HAT library is required to allow the RPi to work with the electronic PCB ‎LED matrix. The following command will install the Sense HAT library with the RPi.‎

Copy Code
sudo apt install sense-hat

To test the software library installation, let’s create a python file to display Hello ‎World on the Sense HAT. Type in the following Linux command to open the nano ‎editor.‎

Copy Code
sudo nano sensehat_test.py

With the nano editor opened, type the following python code into the terminal.‎

Copy Code
from sense_hat import SenseHat
sense = SenseHat()
sense.show_message(“Hello World”)

After the Hello World code has been saved, exit the nano editor. You will execute ‎the code with the following Linux command.‎

Copy Code
python3 sensehat_test.py

The Hello World message will scroll across the Sense HAT LED matrix, as shown ‎below.‎ ‎

text_6

Scrolling Hello World text.‎

You can observe the operation of this scrolling text message here:

 

If the LED matrix does not scroll the Hello World message, there are software and ‎hardware checks that might help. First, press down on the Sense HAT. This will ‎ensure the Sense HAT header is electrically connected to the RPi. You may ‎consider cycling the power of the RPi to properly reset the supporting ‎microcontroller and power supply circuits.‎

A software approach is to type “sudo reboot” into the terminal to reset the Pi. ‎Once the Sense HAT is working correctly, the final step of the project is the ‎installation and execution of the python digital clock software.‎

Installation of the Python Digital Clock Code

Create a filename for the python digital clock code. This python code will be ‎executed from the home/pi directory of the RPi. To create the digitalclock file, ‎type “nano digitalclock.py” into the terminal. With the editor open, type in the ‎digital clock python code as shown here:‎

Copy Code
#!/usr/bin/env python

from sense_hat import SenseHat
import time

sense = SenseHat()

number = [
[[0,1,1,1], # Zero
[0,1,0,1],
[0,1,0,1],
[0,1,1,1]],
[[0,0,1,0], # One
[0,1,1,0],
[0,0,1,0],
[0,1,1,1]],
[[0,1,1,1], # Two
[0,0,1,1],
[0,1,1,0],
[0,1,1,1]],
[[0,1,1,1], # Three
[0,0,1,1],
[0,0,1,1],
[0,1,1,1]],
[[0,1,0,1], # Four
[0,1,1,1],
[0,0,0,1],
[0,0,0,1]],
[[0,1,1,1], # Five
[0,1,1,0],
[0,0,1,1],
[0,1,1,1]],
[[0,1,0,0], # Six
[0,1,1,1],
[0,1,0,1],
[0,1,1,1]],
[[0,1,1,1], # Seven
[0,0,0,1],
[0,0,1,0],
[0,1,0,0]],
[[0,1,1,1], # Eight
[0,1,1,1],
[0,1,1,1],
[0,1,1,1]],
[[0,1,1,1], # Nine
[0,1,0,1],
[0,1,1,1],
[0,0,0,1]]
]

noNumber = [0,0,0,0]

hourColor = [255,0,0] # Red
minuteColor = [0,255,255] # Cyan
empty = [0,0,0] # Black/Off

clockImage = []

hour = time.localtime().tm_hour
minute = time.localtime().tm_min

for index in range(0, 4):
if (hour >= 10):
clockImage.extend(number[int(hour/10)][index])
else:
clockImage.extend(noNumber)
clockImage.extend(number[int(hour)][index])

for index in range(0, 4):
clockImage.extend(number[int(minute/10)][index])
clockImage.extend(number[int(minute)][index])
for index in range(0, 64):
if (clockImage[index]):
if index < 32:
clockImage[index] = hourColor
else:
clockImage[index] = minuteColor
else:
clockImage[index] = empty

sense.set_rotation(90) # Optional
sense.low_light = True # Optional
sense.set_pixels(clockImage)

With the python code typed into the nano editor, save it by exiting out (^Exit) and ‎typing y for yes. To execute the code, enter the following command:‎

Copy Code
 python3 digitalclock.py

Hit the enter key on the keyboard, and you should see the current time displayed. ‎‎(Note, the time will be shown in a 24-hour format.) ‎

To see an update of the time, click the up arrow on the keyboard. The “python3 ‎digitalclock.py” command will be visible in the terminal - hit the enter key to see ‎the updated time. The below picture illustrates the Sense HAT RPi digital clock in ‎operation. ‎

clock_7

A functional Sense HAT -RPi digital clock

A YouTube video clip shows the digital clock working as well:

 

This project was inspired by Steve Amor’s Sense HAT Raspberry Pi development ‎work: https://github.com/SteveAmor/Raspberry-Pi-Sense-Hat-Clock

Référence fabricant SC0329
SENSE HAT 8X8 RGB LED 5 BUT
Raspberry Pi
Référence fabricant SC0442
RASPBERRY PI MOUSE RED
Raspberry Pi
Référence fabricant SC0059
1M HDMI CABLE WHITE (CPRP010-W)
Raspberry Pi
Référence fabricant SC0445
AC/DC WALL MNT ADAPTER 5.1V 15W
Raspberry Pi
Référence fabricant SC0193(11)
SBC 1.5GHZ 4 CORE 2GB PI 4 MOD B
Raspberry Pi
Référence fabricant SC0167
RED USB KEYBOARD
Raspberry Pi
Référence fabricant SC0252L
16GB SD CARD NOOBS SOFTWARE
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.