Digi-Key Corporation Announces Stock on Tyco Electronics G13 Style SMT Assembly and End Cap Cover
THIEF RIVER FALLS, Minnesota, USA - 25 juin 2010
Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, today announced it has stock on Tyco Electronics' G13 style SMT assembly and end-cap cover for the solid state lighting (SSL) industry.
This product is now available for purchase on Digi-Key's global websites and will be featured in future print and online catalogs.
Tyco Electronics' G13 style SMT assembly and end-cap cover supports printed circuit boards (PCBs) and LED strip lighting modules found in the standard T8 and T12 fluorescent LED retrofit tubes.
The integrated assembly enables high-volume manufacturing of fluorescent LED retrofit tubes by allowing a quick SMT electrical connection to the PCB and a standard pin interface to fixture lamp socket (tombstone) connectors.
Designed-in features include a surface mount hold-down to provide additional stability of the connector during insertion and/or extraction of the LED tube. The SMT housing material consists of UL 94V-0 rated high temperature resistant thermoplastic for reflow processing on automated equipment. The end-cap cover interfaces with the connector assembly, heat sink and tube, and is packaged separately for ease of assembly.
Performance characteristics include: 2 Amps current rating, 250 VDC/ 250 VAC voltage rating, 1500 VAC dielectric withstanding voltage and a 0.5 inch pin centerline spacing per G13 specification. Operating temperature ranges from -40 to +120 degrees Celsius. The product is ETL recognized to UL 8750 and UL 1993 standards.
Applications for Tyco Electronics' G13 style SMT assembly and end cap cover include standard T8 and T12 fluorescent fixtures.
About Digi-Key Corporation
Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.
About Tyco Electronics
Tyco Electronics Ltd. is a leading global provider of engineered electronic components, network solutions, specialty products and undersea telecommunication systems, with fiscal 2009 sales of US$10.3 billion to customers in more than 150 countries. We design, manufacture and market products for customers in a broad array of industries including automotive; data communication systems and consumer electronics; telecommunications; aerospace, defense and marine; medical; energy; and lighting. With approximately 7,000 engineers and worldwide manufacturing, sales and customer service capabilities, Tyco Electronics' commitment is our customers' advantage. More information on Tyco Electronics can be found at www.tycoelectronics.com
TE (logo) and Tyco Electronics are trademarks of the Tyco Electronics group of companies and its licensors.
- Editorial Contact
- Laura Stengrim
- DigiKey
- (218) 681-8000 ext. 14489
- laura.stengrim@digikey.com