The New FX888D Soldering Station from American Hakko


Whether setting up a lab for the first time, or replacing old equipment, selecting a new soldering station can be overwhelming. There are plenty of options out there, and while many of them are quality items, it’s hard to know which ones would fit your needs the best.

Thankfully the new FX888D from American Hakko Products Inc. is here to make that selection a little easier. Besides the visually pleasing design, the functionality and reasonable cost make this a new top choice among engineers and beginners alike. It quickly heats to the user-selected temperature preset, has an interchangeable tip, and a low temperature alarm.

The FX888D is a 70 W unit that is easy to use and will get the job done quickly. To see this tool in action, watch our Another Teaching Moment video on the basics of soldering or read about our soldering tips and tricks here. For more information on the FX888D, click here to see the original New Product Discovery video with Randall Restle that introduces the American Hakko Soldering Tool.


À propos de l'auteur

Image of Ashley Awalt

Ashley Awalt est technicienne en ingénierie des applications chez DigiKey depuis 2011. Elle a obtenu sa licence en sciences appliquées en technologies électroniques et systèmes automatisés du Northland Community & Technical College dans le cadre du programme de bourses de DigiKey. Son rôle actuel est d'aider à créer des projets techniques uniques, de documenter les processus et de participer à la production de la couverture médiatique vidéo des projets. Durant son temps libre, Ashley aime - oh, attendez, est-ce qu'on a vraiment du temps libre quand on est maman ?

More posts by Ashley Awalt
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum