LT3042
17
LT3042
17
LT3042
17
3042fb
For more information www.linear.com/LT3042
APPLICATIONS INFORMATION
and ESL tolerance, any non-piezoelectrically responsive 
(tantalum, electrolytic, or film) capacitor can be used at 
the SET pin – although electrolytic capacitors tend to have 
high 1/f noise. In any case, use of surface mount capacitor 
is highly recommended.
Stability and Input Capacitance
The LT3042 is stable with a minimum 4.7µF IN pin capacitor. 
LTC recommends using low ESR ceramic capacitors. In 
cases where long wires connect the power supply to the 
LT3042’s input and ground terminals, the use of low value 
input capacitors combined with a large load current can 
result in instability. The resonant LC tank circuit formed by 
the wire inductance and the input capacitor is the cause 
and not because of LT3042’s instability. 
The self-inductance, or isolated inductance, of a wire 
is directly proportional to its length. The wire diameter, 
however, has less influence on its self-inductance. For 
example, the self-inductance of a 2-AWG isolated wire 
with a diameter of 0.26" is about half the inductance of a 
30-AWG wire with a diameter of 0.01". One foot of 30-AWG 
wire has 465nH of self-inductance. 
Several methods exist to reduce a wire’s self-inductance. 
One method divides the current flowing towards the LT3042 
between two parallel conductors. In this case, placing the 
wires further apart reduces the inductance; up to a 50% 
reduction when placed only a few inches apart. Splitting 
the wires connect two equal inductors in parallel. However, 
when placed in close proximity to each other, their mu-
tual inductance adds to the overall self inductance of the 
wires — therefore a 50% reduction is not possible in such 
cases. The second and more effective technique to reduce 
the overall inductance is to place the forward and return 
current conductors (the input and ground wires) in close 
proximity. Two 30-AWG wires separated by 0.02" reduce 
the overall inductance to about one-fifth of a single wire.
If a battery mounted in close proximity powers the LT3042, 
a 4.7µF input capacitor suffices for stability. However, if a 
distantly located supply powers the LT3042, use a larger 
value input capacitor. Use a rough guideline of 1µF (in 
addition to the 4.7µF minimum) per 8" of wire length. 
The minimum input capacitance needed to stabilize the 
application also varies with the output capacitance as well 
as the load current. Placing additional capacitance on the 
LT3042’s output helps. However, this requires significantly 
more capacitance compared to additional input bypassing. 
Series resistance between the supply and the LT3042 input 
also helps stabilize the application; as little as 0.1Ω to 0.5Ω 
suffices. This impedance dampens the LC tank circuit at 
the expense of dropout voltage. A better alternative is to 
use a higher ESR tantalum or electrolytic capacitor at the 
LT3042 input in parallel with a 4.7µF ceramic capacitor.
PSRR and Input Capacitance 
For applications utilizing the LT3042 for post-regulating 
switching converters, placing a capacitor directly at 
the LT3042 input results in ac current (at the switching 
frequency) to flow near the LT3042. This relatively high 
frequency switching current generates a magnetic field 
that couples to the LT3042 output, thereby degrading its 
effective PSRR. While highly dependent on the PCB, the 
switching pre-regulator, the input capacitance, amongst 
other factors, the PSRR degradation can be easily over 
30dB at 1MHz. This degradation is present even if the 
LT3042 is de-soldered from the board, because it ef-
fectively degrades the PSRR of the PC board itself. While 
negligible for conventional low PSRR LDOs, LT3042’s 
ultrahigh PSRR requires careful attention to higher order 
parasitics in order to extract the full performance offered 
by the regulator. 
To mitigate the flow of high-frequency switching current 
near the LT3042, the LT3042 input capacitor can be entirely 
removed—as long as the switching converter’s output 
capacitor is located more than an inch away from the 
LT3042. Magnetic coupling rapidly decreases with increas-
ing distance. Nonetheless, if the switching pre-regulator 
is placed too far away (conservatively more than a couple 
inches) from the LT3042, with no input capacitor present, 
as with any regulator, the LT3042 input will oscillate at the 
parasitic LC resonance frequency. Besides, it is generally a 
very common (and a preferred) practice to bypass regula-
tor input with some capacitance. So this option is fairly 
limited in its scope and not the most palatable solution.