UDS1100 Quick Start Guide Datasheet by Lantronix, Inc.

View All Related Products | Download PDF Datasheet
LANT?ONIX‘”
2006 Copyright © Lantronix is a trademark of Lantronix. All rights reserved. 900-418 Rev. A 02/06
UDS1100 Quick Start Guide
UDS1100
LANTQON IX”
UDS1100
QUICK START CONTENTS
What’s In the Box . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .2
Pinouts . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .3
IP Addressing . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .4
Connect . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .5
Install the Deviceinstaller GUI . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .5
Assign IP Address . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .6-9
Add the Unit to the Device List . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .10
Configure the UDS1100 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .10
LEDs/Troubleshoot . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .11-12
Contact . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .13
UDS1100
3.: VDC REG we 13 25 1A mm mm) IXVImm m m rx+ rum (Rsrzazc) (R5485/4ZZ) —I
Quick Start Guide
UDS1100
The UDS products allow serial devices to connect and communicate over an
Ethernet network.
This Quick Start explains how to connect, configure, and troubleshoot your
unit using a network connection and our DeviceInstaller software. For more
detailed information or alternative configuration methods, refer to the User
Guide on the CD.
PINOUTS
2WWW.LANTRONIX.COM 3
WHAT’S IN THE BOX
In addition to the UDS, the box contains the following items:
POWER SUPPLY (DOMESTIC UNITS)
PART # COMPONENT DESCRIPTION
520-079-R Power cube, 110 VAC
500-163 Serial Cable
CD
Power Cord Restraint
POWER SUPPLY (INTERNATIONAL UNITS)
PART # COMPONENT DESCRIPTION
520-080-R Power cube, 100-240VAC, with international adapters
500-163 Serial Cable
CD
Power Cord Restraint
DOCUMENTATION:
CD-ROM containing User Guide and software utilities and Quick Start Guide.
a." .. 5 mm: a!» w/umAxE v mum
4WWW.LANTRONIX.COM
CONNECT
Complete the following steps in order. Refer to the numbers in the figure below.
1. Connect a serial device to your unit.
2. Connect an Ethernet cable to the RJ45 port.
3. Supply power to your unit using the power supply that was included in
the packaging.
Note: The required input voltage
is 9-30 VDC (center +) or
9-24 VAC (1.5W maximum
power required).
4. Supply power to the serial device.
INSTALL THE DEVICEINSTALLER GUI
1. Insert the CD into your CD-ROM drive.
If the CD does not launch automatically:
a) Click the Start button on the Task Bar and select Run.
b) Enter your CD drive letter, colon, backslash,
Launch.exe (e.g., E:\Launch.exe).
2. Click the DeviceInstaller button.
3. Respond to the installation wizard prompts.
Quick Start Guide
UDS1100
5
IP ADDRESSING
Your unit must have a unique IP address on your network. Two ways to assign
an IP are described below.
DHCP
Many networks use an automatic method of assigning an IP address called
DHCP. If you are unsure whether your network uses DHCP, check with your
systems administrator.
The UDS looks for a DHCP server when it first powers up.The UDS has acquired
an IP address if the red LED stops flashing and the green Status LED is on
continuously. You can use the DeviceInstaller software to search the network for
the IP your unit has been assigned by the DHCP server and add it to the list of
Lantronix devices on the network.
If the UDS does not acquire an IP, or you do not use DHCP, you must assign a
fixed IP address.
FIXED IP ADDRESS
In most installations, a fixed IP address is desirable. The systems administrator
generally provides the IP address.
The IP address must be within a valid range, unique to your network, and in the
same subnet as your PC.You will need the following information before you set
up the unit as described in Assign IP Address.
IP Address:
___ ___ ___ ___
Subnet Mask:
___ ___ ___ ___
Gateway:
___ ___ ___ ___
Ethernet, Power, and Serial Connections
ASSIGN IP ADDRESS CONTINUED…
3. Enter the hardware or Ethernet address of the device. The address is on the
label on the underside of the unit.
4. Select Assign a specific IP address to assign a static IP address to the device,
or select Obtain an IP address automatically to enable BOOTP, DHCP, or
Auto IP on the device. Click Next.
6WWW.LANTRONIX.COM
Quick Start Guide
UDS1100
7
ASSIGN IP ADDRESS AND NETWORK CLASS
1. Click the Start button on the Task Bar and select Programs Lantronix
DeviceInstaller DeviceInstaller. The DeviceInstaller window displays.
2. Click the IP icon .The Device Identification window displays.
Figure 1. DeviceInstaller Window
Figure 2. Device Identification
Figure 3. Assignment Method
8
Quick Start Guide
UDS1100
WWW.LANTRONIX.COM 9
ASSIGN IP ADDRESS CONTINUED
6. Click the Assign button to finalize the IP assignment.
ASSIGN IP ADDRESS CONTINUED…
5. Enter the IP address, Subnet mask, and Gateway being assigned to the
device in XXX.XXX.XXX.XXX format. Click Next.
Figure 5. Assignment
Figure 4. IP Settings
Web Corliguation ‘I Telnet Configuralion
10
Quick Start Guide
UDS1100
WWW.LANTRONIX.COM 11
LEDS/TROUBLESHOOT
The unit contains the following LEDs:
• Power
• 10/100 Mb Link
• 10/100 Activity
• Diagnostics
• Status Channel 1
Simultaneously lit red and green LEDs means something is wrong. If the red
LED is lit or blinking, count the number of times the green LED blinks between
its pauses.The following table explains the LED functions.
ADDING THE UNIT TO THE DEVICE LIST
Now add the unit to the list of similar Lantronix devices on the network
so that you can manage and configure it.To perform this step, click the
Search icon . DeviceInstaller locates the unit and adds it to the list.
CONFIGURATION
Once the UDS is in the device list, it can be configured.
1. Double-click the unit in the list. Details about the unit display.
2. Select one of the following tabs:
Note: For details about configuration settings, see the UDS User Guide.
12
CONTACT
For questions and technical support, please check our online knowledge base
at www.lantronix.com/support
Lantronix
15353 Barranca Parkway, Irvine, CA 92618, USA
Phone:(949) 453-3990 or Fax: (949) 453-3995
www.lantronix.com
WWW.LANTRONIX.COM 13
Quick Start Guide
UDS1100
SERIAL LEDS MEANING
10/100 Mb Link steady green
Valid network connection
10/100 Activity blinking
Network packets transmitting and receiving
Diagnostic steady red and
3 blinks = Network controller error
status blinking green
4 blinks = EEPROM checksum error
5 blinks = Duplicate IP address on network
Diagnostic blinking red and
5 blinks = No DHCP response
Status blinking green
Status steady green Serial port not connected to network
Status blinking green Serial port connected to network

Products related to this Datasheet

ETHERNET TO SER RS-232/422/485